Generating Insights: Alternative Fuels

Powering the alternative fuels and hybrid revolution Over the past 20 years, the world has started shifting away from fossil fuels towards decarbonised power. Energy producers are increasingly em...

Generating Insights: Changing the Fields: An Electromagnetic Design Perspective

Electromagnetic design is right at the core of the product design stage in alternators and can mean the difference between releasing a good product and a great product. The expertise we have at S...

Generating Insights: Best practices for re-lubricating alternator bearings

Grease is a form of lubrication that is fundamental to the operation and longevity of rolling element bearings. This form of lubrication reduces direct metallic contact between the bearing’s race...

Generating Insights: Alternator Life - Codes & Standards

STAMFORD | AvK products have an expectation from their customers that they are both reliable and durable: they expect it to deliver a lifetime of performance without any failure. However, it is r...

Generating Insights: Bearing Life

One of the most important components of the alternator, is the shaft bearings STAMFORD | AvK has a proven track record of manufacturing and supplying superior alternators for numerous a...

Generating Insights: UL Certification

Underwriters Laboratories (UL) is an independent organisation that certifies, tests, inspects and audits for product compliance. UL is chiefly concerned with the safety aspects of products. Manuf...

Generating Insights: Overview of Rating Definitions for Alternators and Generator Sets

The KVA rating placed on an alternator is governed primarily by the thermal capabilities of the winding insulation system The rating on an alternator defines its capability to deliver electrical ...

Generating Insights: Environmental Impact

Globalisation and the advancements in transportation and logistics has enabled us to address the growing demand by setting up ad-hoc power plants using reciprocating engine driven gensets; this h...

Generating Insights: Insulation Classes and Life Expectancy

This article explains the meaning of thermal classes and temperature rises and provides an overview of the half-life expectancy of an insulation system.Thermal/Insulation Classes The definition o...

Generating Insights: Principles of Shaft Alternators in Marine Applications

Application overview In marine applications, Shaft Electrical Machines (SEM’s) are connected to the vessels propulsion engine and are often required to operate in a multi-function role. They oper...